Containers
Use container objects to structure your application and create user interface navigation.
Object | Description |
---|---|
Container for objects that constitute a specific widget. By default, each new panel has a fixed width and height and is aligned with the top-left corner of the parent object. | |
Container for objects that constitute a specific interface. By default, each new screen stretches to cover the entire parent object. | |
Panel that automatically arranges objects horizontally next to each other. | |
Panel that automatically arranges objects vertically next to each other. | |
Panel that automatically scales its children objects when the container aspect ratio changes. | |
Panel that displays other panels based on the application logic. | |
Panel that contains other panels and automatically organizes panels into tabs that you can navigate. | |
Button that opens and closes a panel when selected. | |
Root container. In a Presentation Engine, you can set Window to specify the initial user interface at runtime. | |
A modal window that does not allow interaction with other interface components until it is closed. | |
A window that displays in response to an event. | |
Panel that can scroll to display content larger than the panel size. | |
Container that includes expandable content blocks. |
Provide Feedback