- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Add an Advanced SVG image
Add an Advanced SVG image to the canvas to change the properties of individual image parts at design time or runtime.
TIP:
For example, you can signal a hardware part malfunction by highlighting a hardware component representation.
Prerequisites
To control the image properties, obtain an SVG file that conforms with these requirements:
- File format is SVG 1.2 Tiny
- Fill and stroke properties exist and have colors defined as XML attributes or inline CSS
- Color values are hexadecimal
TIP:
If the SVG file does not conform with the requirements, the image will display as expected, but you will not be able to change the image properties.
- To add an Advanced SVG image
- InProject view, right-click the object or folder to contain the image and then select .
- Double-click the empty imagethat appears on the canvas.
- InSelect file, select the image to display and then chooseSelect.TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand inImport file(s)Import file(s), select the file to import and then chooseSelect.
- (optional) Open the SVG file in a text editor and verify the@idattribute of the image element that you want to change.For example:<g id="ConveyorChassis"> <polygon style="fill:#3C4660;" points="8.532,379.733 503.466,379.733 503.466,277.333 8.532,277.333"/> </g>
- InProperties, underProperty, from the#IDselect the image element to change.TIP: The dropdown options correspond with the@idattributes of the SVG file elements. If values do not appear in the dropdown, the SVG image may not conform with the requirements needed to control the image properties.
- InValue, either:
- Enter a hexadecimal color value.
- Create a complex dynamic link with a converter to hexadecimal color values.Complex dynamic link example
Advanced SVG image example - disabled alarm (gray conveyor chassis)

Advanced SVG image example - enabled alarm (red conveyor chassis)

For more information, see Develop an icon that changes color.
Provide Feedback