Change the appearance of a drawing object
Change the properties of a drawing object to change the appearance of the object.
TIP:
To specify property values, you can double-click an existing value to type the numeric value of the value of the property or select
to navigate to and select the tag in the controller. The value of the tag is then the value for the property. To change a color property, in

Add Dynamic Link
Properties
, you can select the color block to open Select Color
and drag to select the new color.- InProject viewor in the editor, select the drawing object.
- InProperties, expand theAppearancecategory and change the properties. The selected drawing object determines the displayed properties:
- Border color. Specify the color of the border of the object.
- Border thickness. Specify the thickness of the object border in pixels.
- Fill color. Select the fill color of the object.
- Opacity. Select the opacity of the drawing object. Specify 0 to make the object transparent.
- Rotation. Specify the rotation of the object around the center point. Positive values indicate clockwise rotation in degrees.
- Thickness. The thickness of the pen line that draws the object.
- Visible. Specify whether the drawing object is visible at runtime. SelectTrueto make the object visible orFalsenot to have the object visible at runtime.
Provide Feedback