- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Draw a line
Use the
Line
tool to draw a line.- InProject view, double-click the container to include the object.
- In the editor toolbar, selectLine.
- In the editor, position the crosshair where the line, polyline, or polygon is to begin.
- Drag to draw the line.
The object appears in the editor and in
Project view
.Provide Feedback