Configure presentation engines
Add a native presentation engine or a web presentation engine to your project.
TIP:
Each project can contain a single native presentation engine and a single web presentation engine. If your project runs on the Embedded Edge Compute Module (1756-CMEE1Y1), add a web presentation engine and delete the native presentation engine.
- InProject view, right-click a window object.
- Select one of the following options:
- To create a native presentation engine, select.
- To create a web presentation engine, select.
- To delete a presentation engine, right-click a presentation engine and selectDelete.
- (optional) InProperties, edit the presentation engine options.
Provide Feedback