- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Implement the UIPopulator NetLogic
Point the NetLogic to the graphic objects.
- InProject view, selectUIPopulator.
- InProperties, at the top, selectand selectVariable.
- Hover-over the variable, select, and enterModelObject.
- Next toModelObject, selectInt32and selectNodeId.TIP: If you do not see the required option, select theShow allcheckbox.
- Create a dynamic link betweenModelObjectand .
Provide Feedback