- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Communicate with Azure IoT Hub broker
Azure IoT Hub supports sending or receiving information only on specific topics of a device.
Prerequisites
Azure IoT Hub does not allow you to send and receive information on custom topics. A device can send or receive information only on specific topics of the device:
- send
- devices/deviceid/messages/events/
- receive
- devices/deviceid/messages/devicebound/#
- To communicate with Azure IoT Hub broker
- For each client that to send or receive messages, create a device on the Azure IoT Hub.TIP: Clients cannot use the same devices to send or receive data.
- Verify that sending and receiving messages is successful.TIP: The Device Explorer and Azure IoT Explorer applications enable you to monitor the received messages and send messages to devices.
Provide Feedback