- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Libraries
Libraries contain object definitions that you can add to your projects.
Library types
Type | Description |
---|---|
Template library | The default library of objects that you cannot edit or remove. Template libraries are provided for:
|
Custom library | A library created by a user that contains a set of objects either curated from the template libraries or customized for specific automation scenarios. |
TIP:
To find a template quickly, select any item under
Components
and start typing.Library repositories
You can store libraries locally or in a remote Git repository. Libraries are available across
FactoryTalk Optix
projects.Libraries are saved in the folder.
C:\Users\
UserName
\Documents\Rockwell Automation\FactoryTalk Optix\LibrariesLibrary updates
Libraries and library objects are tied to the version of the
FactoryTalk Optix
software with which they were originally configured. When you install an updated version, FactoryTalk Optix
updates the built-in template libraries to make the libraries compatible with the new software.If your project contains custom libraries that use components that changed in the updated version of
FactoryTalk Optix
, you must manually update the custom libraries.Provide Feedback