Import a template

Import a template

Place a template in a node in
Project view
to add the object, object type, or a variable to the project.
TIP: If the template is a graphic object, you can drag the graphic element from the library to the editor.
  1. From the main toolbar, select
    Template Libraries
    and either:
    • Drag a template from the library into a node in
      Project view
      .
    • Drag a graphic object template from
      Libraries
      to the editor or
      Project view
      .
  2. If the template is an object type, select either:
    • Import as type
      . Add an object type based on the template into the project.
    • Import as instance
      . Add an object instance based on the template into the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal