Create a template
Use a template to create objects, object types, and variables that have similar attributes.
- SelectTemplate Libraries
- FromProject view, drag the node into a library inTemplate Libraries.For example, drag an object, object type, variable, or widget.A new template appears underComponents.
- (optional) Select the template and enter a description.For example, explain how to use or implement the object, object type, variable, or widget.
Provide Feedback