- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Connect to remote access
Configure remote access to the device as well as remote assistance through the
FactoryTalk Remote Access
Widget.- On the device, open the screen with the FactoryTalk Remote Access Widget.If you created your project using the OptixPanel template on the start page, selectSettingsand then selectFT Remote AccessOn theConnectionstab of the widget,FT Remote Access runtime versiondisplays the version that is running on the device.
- To connect the device to theFactoryTalk Remote Accessapplication, selectConnections.
- UnderFT Remote Access connection, selectConnect.If your device is already added to theFactoryTalk Remote Accessdomain, the device is automatically connected. If your device is not in theFactoryTalk Remote Accessdomain, you are prompted to add your device in FactoryTalk Remote Access with the displayed device id and password.
Provide Feedback