- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Deadband interval configurations
The deadband helps prevent sampling values in rapid succession due to oscillation in the control system.
Sampling type | Deadband settings |
---|---|
Any change from the previous sample | Default deadband mode = None |
Absolute value of change from the previous sample is equal to or greater than a specific value |
|
Percentage of change from the previous sample is equal to or greater than a specific value |
|
Provide Feedback