- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Delete an event logger
Delete an event logger by removing the event logger object in
Project view
.
TIP:
You can disable an event logger without the need to completely remove the logger from the project. For more information, see Edit an event logger.
- InProject view, right-click an event logger object and selectDelete.
Provide Feedback