View type instances
View instances of a type, such as a window, to view all instances in the information model where the type exists.
- InProject view, navigate to and right-click the type and then selectShow Instances.
- InInstances of (name), select an instance of the type and selectGo to ...
FactoryTalk Optix Studio
navigates to the instance of the type. Objects referenced in a NetLogic are not shown.Provide Feedback