Create an object type
When you create an object type, the original object from which you create the type becomes an instance of the new type.
- FromProject view, drag an object into a folder inType view.
- (optional) InProperties, select , selectDisplay name, and enter the display name.
- (optional) InProperties, select , selectDescription, and enter the description.
The new object type appears in
Type view
and Project view
. The hover-over tooltip shows the display name and description.
Provide Feedback