- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create an object
Create an object to add a node to the project.
- InProject view, select the folder in which to create the object, and then selectin theProject viewtoolbar.TIP: You can also right-click a folder inProject viewand use theNewcontext menu to create objects.The context menu displays objects that the folder can contain based on the folder category.
- Select the object to add to the project.
- (optional) InProperties, select, selectDisplay name, and enter the display name.
- (optional) InProperties, select, selectDescription, and enter the description.
The new object appears in
Project view
. The hover-over tooltip shows the display name and description.
Provide Feedback