Create a node pointer
Create a node pointer in
Project view
to reference to another node of the project.- InProject view, select the folder or object to contain the variable.
- InProperties, create a dynamic link to the node to point to.For more information about dynamic links, see Create dynamic links.
- (optional) expandNodePointerand complete these properties:#
- Kind. The kind of the node that the node pointer targets.
- Node class. Either:
- Instance
- Type
- Any
- (optional) InProperties, select , selectDisplay name, and enter the display name.
- (optional) InProperties, select , selectDescription, and enter the description.
Provide Feedback