Create a variable type
Create a variable type in
Project view
. You can then create variables of the variable type.- FromProject view, drag an existing variable into a folder inType view.The variable type appears in bothType viewand in theProject viewfolder that has the same name as the folder inType view.TIP: The variable inProject viewis appended with(type)and the original variable that you dragged fromProject viewis now an instance of the type.
- (optional) InProperties, select , selectDisplay name, and enter the display name.
- (optional) InProperties, select , selectDescription, and enter the description.
Provide Feedback