Close a project
Close a project from the Start page.
You can have more than one project open at a time. When you open additional projects, additional instances of
FactoryTalk Optix Studio
open.- From the main toolbar, select. On the Start page, selectProjectClose.TIP: If you open the Start page from an open project and want to close the Start page, select
.
Provide Feedback