Create a project

Create a project

A project contains elements with which a
FactoryTalk Optix Application
is made. You can create either a local project or a project from a remote location.
  1. In the main toolbar, select
    Project
    .
    The Start page opens.
  2. Select
    New
    .
  3. To create a local project that has a default window and configured categories in
    Project view
    , select the project type: .
    • Default
      . Create a project with all categories and a main window in
      Project view
      .
    • OptixPanel
      . Create a project with all categories and a main window in
      Project view
      , in addition to:
      • A
        System
        object with a pre-configured
        FT Remote Access
        widget to request access to the FactoryTalk Remote Access server and assistance from the FactoryTalk Remote Access application.
      • A
        SettingsWidgets
        folder that contains
        Network Settings
        ,
        Device Settings
        ,
        Date & Time
        , and
        Load Application
        widgets.
      • A main window that displays and allows you to navigate the default widgets at runtime as well as place your own content on the Home page of the window.
      • Automatic language switching for widgets.
      • An enabled virtual keyboard
    To create a blank project that has no default content, in
    FactoryTalk Optix Studio Options
    , select
    Advanced mode
    and then restart
    FactoryTalk Optix Studio
    to select
    Blank
    on the Start page. See Set options.
  4. In
    Name
    , type the name of the project.
  5. In
    Location
    , type the path to the project.
    The default location is
    C:\Users\
    UserName
    \Documents\Rockwell Automation\FactoryTalk Optix
    . Select
    Browse files
    to browse for a different location.
  6. (optional) Select
    Use version control
    .
    With version control enabled, you can back up the state of your project to a local repository and push local changes to a remote repository.
  7. (optional) Select
    Encrypt secrets
    to encrypt project passwords, custom objects that have the
    Password
    DataType, and
    YAML
    files that represent the project information model.
    To enable the
    Encrypt secrets
    option, log in to
    FactoryTalk Hub
    . For more information, see Project secrets encryption.
  8. Under
    Set main window size
    , specify the width and height of the main window when you create projects. Accept the default
    Custom
    window size, enter a new
    Width
    and
    Height
    for a new custom window size, or select a pre-configured window size or OptixPanel if you are creating an OptixPanel project.
    The default custom window size is 400 x 400 pixels.
  9. Select
    Create
    .
  10. (optional) To create a project from a remote location:
    1. Select
      Remote
      .
    2. In
      Remote URL
      , enter the URL of your remote repository supplied by your System Administrator to specify the remote project that you want to open.
    3. In
      Location
      , enter the folder on your local computer where you will save and commit changes before pushing them to the remote repository.
    4. Select
      Open
      .
      If you are signed in to
      FactoryTalk Optix
      , you do not have to know the
      Remote URL
      or
      Location
      .
      Create a new project
      automatically displays all of the potential repositories accessible with your GitHub account and all of the remote projects that you can open.
      Opening project from remote
      appears in the status bar and the new project opens with the same name as the remote repository.
The new project opens. If there was an existing project open, the project opens in a new instance of
FactoryTalk Optix
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.