Restore a project
If a project is corrupted or unwanted changes are saved, you can restore an earlier version of the project.
Ensure that the project is closed in the
FactoryTalk Optix Studio
.- From the%localappdata%\Rockwell Automation\FactoryTalk Optix\Studio\Backups\[Project Name]folder, copy the entire folder of the desired backup.
- Replace the current project folder with the backup folder.
- Open the project and verify that it is restored successfully.
Provide Feedback