Manage recipes at runtime

Manage recipes at runtime

Use the recipes editor widget to store a new recipe, to delete an existing recipe, or to apply a recipe on the controller.
When the user creates, edits, or loads a recipe from the database at runtime, an alias to the
Edit model
node is automatically created in the root project node. The alias node has the same name as the recipe schema it refers to. Until the node is saved, deleted, or sent to the controller, it contains a temporary copy of the created, edited, or loaded recipe data.
IMPORTANT: If the
FTOptixApplication
execution stops, the
Edit model
node and its data are deleted.
  • To manage recipes at runtime
  • To store a new recipe:
    1. Edit the values of the ingredients.
    2. In the recipe list, enter a name for the recipe.
    3. Select
      Save
      .
  • To delete a recipe, select a recipe and select
    Delete
    .
  • To apply a recipe on the controller:
    1. Select a recipe.
      Recipe ingredients values display.
    2. Select
      Apply
      .
      In the right column, ingredients values loaded to the controller display.
    3. To change the values of the ingredients on the controller, edit the values, select
      Save
      and select
      Apply
      .
      The values of the ingredients on the controller update in the right column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal