- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure idle Timeout
You can configure a timeout when there is a lack of user activity in the
FactoryTalk Optix
. A timeout can trigger any custom event. To configure a timeout, the application must have interactive graphic objects. At runtime, inactivity includes a lack of cursor movements, keyboard actions, and user interactions.
You can configure an idle timeout for either a specific page or an entire session.
Provide Feedback