User locale configuration

User locale configuration

The user locale is personal data that specifies the session locale at runtime. Set the user locale in the
Locale
property of the
User
object.
If the
FactoryTalk Optix Studio
does not support the main locale, use C# to have APIs return nodes and set multiple locales for the same user. The order of user locales determines the priority for the session locale.
When the session locale is set automatically at runtime based on the user locale and no user locales are configured, the session uses a fallback locale.
TIP: Use the
Session UI
object to manage the session locale for a multilingual project that does not have user locale information. The user must then select the locale at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal