Change the interface language

Change the interface language

Change the interface language to display a different language throughout the
FactoryTalk Optix Studio
application at design time and runtime.
  • To change the interface language, either:
    • In
      Project view
      , select the project node and then in
      Properties
      , expand
      Localization
      and in
      Locales
      , select the language.
    • Select
      FactoryTalk Optix Studio Options
      and then in
      Language and Locale
      , select the language.  
    • Have a different user with a different associated locale language log on.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal