- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a localization dictionary
Create a localization dictionary to display application content in the language where the user is located. The localization dictionary contains all of the translated strings in the different languages. You can then select a language to display for the application at both design time and runtime.
NOTE:
When a localization dictionary exists for your project, it impacts all variables with
LocalizedText
data type. When you enter a value for a variable which value data type is LocalizedText
, a suggestion box displays containing possible matches to the key you entered. You can select a suggestion and confirm with ENTER, or you can press ESC to close the suggestion box, and press ENTER to insert the text you entered as-is. If you create a project in
FactoryTalk Optix Studio
using a standard template, the Translations
folder contains a localization dictionary by default.- InProject view, right-clickTranslationsand then selectNew.
The
LocalicationDictionary#
appears in the Translations
folder. Provide Feedback