- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure security for content at runtime
Configure the security of a screen or content at runtime for users in a group or role. For example, specify whether a screen or content is Visible or Enabled by creating a dynamic link from those properties to a group or role Session variable.
Create users and groups or roles and then assign users to groups or roles.
- InProject view, select the screen or graphic object.
- InPropertieshover over the property and then select.Add Dynamic Link
- In the dynamic link browser, expandAliases > Session > Session.
- Set the value of the property for a:
- Group. ExpandGroupsand select the group.
- Role. ExpandRolesand select the role.
TIP: To set the same property value for additional groups and roles, in the property, create a complex dynamic link with an expression evaluator or other necessary logic. See Create a complex dynamic link.
Provide Feedback