- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Delete a user
Delete a user to no longer have the user be a user of the project.
Delete a user from either the dashboard page or
Project view
.- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, underUsers, select the users to delete.
- SelectDelete.TIP: You can also right-click the user to delete from eitherManage users and groupsorProject view, and then selectDelete.
The user is removed from the dashboard page and
Project view
. If the user was assigned to a group, the user no longer appears as a member of the group.Provide Feedback