Create objects
Use C# APIs to create objects in the
FactoryTalk Optix Studio
project and return the corresponding C# objects.The APIs are supplied by the
InformationModel
class, displayed by the FTOptix.HMIProject
module.Provide Feedback