- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
IUAVariable.RemoteRead(timeoutMilliseconds)
Returns the value of the variable on which it invokes. The optional argument sets the timeout period.
UAValue RemoteRead(doubletimeoutMilliseconds);
Arguments
- timeoutMilliseconds(double)
- The timeout period, expressed in milliseconds, after which the API throws an exception.TIP: If not specified, the default value of the argument is30000(30 seconds).
Returns
- UAValue
- The value of the variable.
Example
In the following example, the
Speed
variable value is read and given in an information message.
var currentSpeed = Project.Current.GetVariable("Model/Motor/Speed"); var value = currentSpeed.RemoteRead(); Log.Info(value.ToString());
Provide Feedback