- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Sort project nodes
You can use C# to sort nodes within the parent node through the
MoveUp()
and MoveDown()
methods.Methods
You can invoke these methods on a node:
- MoveUp()
- Moves the node up by one position with respect to the sister nodes within the parent node.Invoking theMoveUp()method on the first node within the parent node has no effect.
- MoveDown()
- Moves the node down by one position with respect to the sister nodes within the parent node.Invoking theMoveDown()method on the last node within the parent node has no effect.
Graphic objects considerations
If you sort graphic objects with the
MoveUp()
and MoveDown()
methods:
- The methods only have an effect if invoked on a graphic object within a type (for example aPanel (type)).
- To see the function effect on the graphic, reload the page manually.
Provide Feedback