- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Prepare the remote machine for debugging
Install and configure the Remote Debugger desktop application.
Prerequisites
Download and install Visual Studio Debug Tools from Remote Debug a C# or VB project - Visual Studio (Windows) | Microsoft Docs.
- To prepare the remote debugging target machine
- Open the Remote Debugger desktop application.
- Observe the device and port to connect to the remote debugging target.
- Configure the firewall. See Remote Debug a C# or VB project - Visual Studio (Windows) | Microsoft Docs.
Provide Feedback