- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Edit a NetLogic
Modify the NetLogic code by using an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
- To edit a NetLogic
- InProject view, double-click a NetLogic object.The default external code editor opens.TIP: Rockwell Automation recommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.
- In the external code editor, edit the NetLogic code and save the file.TIP:You can expose custom methods by adding such declarations:[ExportMethod] public void MyCustomMethod1() { //Add custom code here }
Provide Feedback