- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Integrate the interface with the NetLogics
Integrate the NetLogics with the application interface.
- InProject view, expand .
- Configure the Insert Random Data button:
- InProject view, selectInsertButton.
- InEvents, next toMouseClick event, selectand select .
- Configure the Display Query in Label button:
- InProject view, selectRunQueryButton.
- InEvents, next toMouseClick event, selectand select .
Provide Feedback