- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Start page
The Start page opens when you launch
FactoryTalk Optix Studio
to create or open a project.The Start page allows you to open and create projects using three views:
Home
Create a
Default
project that contains all Project view
categories and a preconfigured main window or create an OptixPanel
project that contains preconfigured widgets for that device. You can search for a recent project or filter projects to see local or remote projects.New
Create a
Default
project that contains all Project view
categories and a preconfigured main window or create an OptixPanel
project that contains preconfigured widgets. When creating a new project, use version control to create committed versions of the project that you can later compare and restore. Open
Open a recent or remote project. When opening a remote project, enter a
Remote URL
to clone a repository and create a project with the same name as the repository, or enter a Location
to open an existing project in the remote repository. Provide Feedback