Configure an alarm grid
Add a table that displays alarms status in real time.
- From the toolbar, select.Template Libraries
- InLibraries, search forAlarm Grid.
- UnderComponents, dragAlarm GridontoPage2 (type)inProject view.AlarmGrid1appears underPage2 (type).
- SelectClose.
- InProject view, selectAlarmGrid1.
- InProperties, setHorizontal alignmenttoStretch.The object adjusts its width to the container at runtime.
AlarmGrid1 in Page2
![](/content/dam/dita/en/factorytalk-optix/1-3-2/_images/quick_start_alarm_grid.png/_jcr_content/renditions/original)
Provide Feedback