FactoryTalk Optix Studio web editor

FactoryTalk Optix Studio web editor

You can use
FactoryTalk Optix Studio
in a web browser through
FactoryTalk Hub
.

Editor features support

FactoryTalk Optix Studio web editor
supports all
FactoryTalk Optix Studio desktop editor
features except for:
  • Save logs from the
    Output
    tabs.
  • Edit NetLogic files.
  • Open
    FactoryTalk Optix
    Help.
  • Display paths in logs in the
    Output
    tabs.
  • Add files and images by dragging and dropping them into
    FactoryTalk Optix Studio web editor
    .
  • Restart the application at runtime by using the
    Commands
    Core commands
    Restart
    method.

Emulator features support

FactoryTalk Optix Studio web editor
emulator supports all features of
FactoryTalk Optix Studio desktop editor
emulator except for:
  • Control the
    WebBrowser
    object in the runtime emulator.
  • Control the
    PDFViewer
    object in the runtime emulator.
  • Control the
    Video
    object in the runtime emulator.
  • Control the
    Window
    object in the runtime emulator.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal