Develop a button that replaces an SVG image

Develop a button that replaces an SVG image

Create a button and NetLogic that modifies an SVG image at runtime.
NOTE:
Download a sample project:
ReplaceImage.zip
Application example
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal