- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Certificate errors
Certificate errors may display when using the web browser object.
Certificate errors that are ignored at runtime when
Ignore invalid CA errors
is set to True
. For more information, see Configure a web browser.Error | Description |
---|---|
CertificateAuthorityInvalid | Certificate not signed by a trusted CA |
Certificate errors listed in
Certificate error
. To ignore the errors, select Accept the risk and continue
at runtime.Error | Description |
---|---|
SslPinnedKeyNotInCertificateChain | Certificate does not match the built-in public keys pinned for the host name |
CertificateCommonNameInvalid | Certificate common name does not match host name |
CertificateDateInvalid | Certificate is not valid at the current date and time |
CertificateAuthorityInvalid | Certificate not signed by a trusted CA |
CertificateContainsErrors | Certificate contains errors |
CertificateNoRevocationMechanism | Unable to determine if the certificate is revoked |
CertificateUnableToCheckRevocation | Unable to get revocation information for the certificate |
CertificateRevoked | Revoked certificate |
CertificateInvalid | Invalid certificate |
CertificateWeakSignatureAlgorithm | Certificate signed with a weak signature algorithm |
CertificateNonUniqueName | Certificate host name is not unique |
CertificateWeakKey | Certificate contains a weak key |
CertificateNameConstraintViolation | Certificate claimed DNS names violate name constraints |
CertificateValidityTooLong | Too long certificate validity period |
CertificateTransparencyRequired | Unable to get required certificate transparency information from the server |
CertificateKnownInterceptionBlocked | Certificate known for interception by an entity other than the device owner |
Provide Feedback