- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Manage file and resource paths
The
ResourceURI
static C# class represents the path (URI) of a file or resource inside or outside the project.
TIP:
The
ResourceURI
class represents the same type of data for the variables. For example, the Path
property of an Image
object.ResourceURI object properties
ResourceURI
object propertiesThe following table shows the
ResourceURI
class properties and the methods that the class exposes to reference files or resources.Properties | Data type | Description |
---|---|---|
URIType | URIType | The path type of the path contained:
|
ProjectRelativePath | string | The relative path of a file in relation to the ProjectFiles folder. |
ApplicationRelativePath | string | The relative path of a file in relation to the ApplicationFiles folder. |
AbsoluteFilePath | string | The absolute path of a file external to the project. |
URI | string | The absolute path of a generic resource. |
Depending on the value of the
URIType
property of an object of the ResourceURI
type, other properties may or may not expose a value.URIType | ProjectRelativePath | ApplicationRelativePath | AbsoluteFilePath | URI |
---|---|---|---|---|
URI | - | - | - | URI (for example, a URL HTTP) |
ProjectRelative | Relative path to the ProjectFiles folder | - | - | Absolute path |
ApplicationRelative | - | Relative path in relation to the ApplicationFiles folder | - | Absolute path |
AbsoluteFilePath | - | - | Absolute path | Absolute path |
Provide Feedback