- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Edit the localization dictionary
Add the Polish (pl-PL) locale and localize the strings.
- InProject view, expand theTranslationsfolder.
- Double-clickLocalizationDictionary1.
- Add the pl-PL locale. See Add a locale language to a localization dictionary.
- Localize strings. See Translate a string.
Provide Feedback