- FactoryTalk Optix Studio setup
- FactoryTalk Optix Runtime setup
- FactoryTalk Optix Runtime entitlements
FactoryTalk Optix Runtime setup
Calculate the size of Runtime package size that you need for your device, then download and activate it. You can activate
FactoryTalk® Optix™
Runtime on either an online or offline device.Provide Feedback