Download Runtime Tools on the device
FactoryTalk® Optix™
Runtime Tools are required on any device running a FactoryTalk® Optix™
application.They include the
FactoryTalk® Optix™
Entitlement Manager and FactoryTalk® Optix™
Application Update Service.Runtime Tools are embedded in OptixPanel
™
Graphic Terminals by standard, so you do not need to download and install them.If you are using a Runtime device, download Runtime Tools from the
FactoryTalk® Optix™
landing page. You can download and install Runtime, including License Manager.- Access theFactoryTalk® Optix™landing page. See FactoryTalk Optix landing page.
- On theFactoryTalk® Optix™landing page, selectRuntime Tools.
- Scroll down toRuntime Tools Releaseto view the Runtime Tools released versions.
- (optional) To view theFactoryTalk® Optix™release notes, selectRelease Notes.
- (optional) To view the latest changes inFactoryTalk® Optix™, selectChangelog.
- (optional) To search for a specific Runtime Tools release, type the release number inSearch.
- To download a specific Runtime Tools release, selectDownloadafter the desired version number, .
- Select the checkbox next to theFactoryTalk Optix Runtime Toolsinstallation package and click on the first instance of the
symbol in the upper right corner. Eventually, click on
Download Now. - Scroll to read the EULA and selectAccept and Download.
- Install theRockwell Automation Download Managerlocated in your Downloads folder. To do so, select
.
Rockwell Automation Download Managerinstalls, runs, and download the Runtime Tools into the specified folder. Download progress is displayed in theRockwell Automation Download Manager. - To determine the Runtime Tools downloading path, after the path, selectChangeto select a different folder.
- Runtime Tools are ready for installation.
Provide Feedback