- FactoryTalk Optix Studio setup
Rehost a FactoryTalk Optix Studio Pro entitlement
You can rehost the
FactoryTalk® Optix™
Studio Pro entitlement by using either the FactoryTalk® Optix™
Studio desktop application or the FactoryTalk® Optix™
landing page.Follow one of the following procedures to reallocate a
FactoryTalk® Optix™
Studio Pro entitlement from a user to another.Rehosting from the desktop application
- Make sure that your device is connected to the Internet.
- Access theFactoryTalk® Optix™Studio desktop application.
- Click theLoginicon at the top right corner.
- On the drop-down menu, selectRehost entitlement.
Rehosting from the FactoryTalk® Optix™ landing page
FactoryTalk® Optix™
landing page- Make sure that your device is connected to the Internet.
- Access theFactoryTalk® Optix™landing page.
- Select.
- Click theRehostbutton located in the rightmost column next to theFactoryTalk® Optix™Studio Pro entitlement that you want to rehost.
Provide Feedback