Start FactoryTalk Optix Studio Pro
Once an entitlement has been allocated, you can launch
FactoryTalk® Optix™
Studio Pro from either your desktop or a web browser, having the Pro features enabled in either way.
NOTE:
You can use
FactoryTalk® Optix™
Studio Pro if you have been assigned an entitlement or granted a 90-day trial period.- Launch:FactoryTalk® Optix™Studio Pro from your desktopIMPORTANT: Despite the application icon on the desktop remains unchanged, the Pro features will show up upon valid user login and entitlement allocation.
- In the WindowsStartmenu, start typingFactoryTalk Optix Studioor double-click theFactoryTalk® Optix™Studio icon on your desktop.
- Once the application opens, if you are not signed in, selectSign infrom the top bar and sign in with your MyRockwell account credentials.
- If you made any changes to your entitlements while working withFactoryTalk® Optix™Studio, restart the application.
- Launch:FactoryTalk® Optix™Studio Pro from a web browser
- Access theFactoryTalk® Optix™landing page. See FactoryTalk Optix landing page.
- Authenticate as required. See Authenticate your FactoryTalk Hub account.
- On theFactoryTalk® Optix™landing page, selectOpen in Browser.TIP:If you do not have an entitlement forFactoryTalk® Optix™Studio Pro, a dialog displayingEntitlement requiredopens.CompleteName,Email, andDescriptionand then selectSubmit.You will receive an email to grant you a trial entitlement when your request is approved. Approval can take up to 24 hours. You can download and install the desktop version ofFactoryTalk® Optix™until yourFactoryTalk® Optix™Pro entitlement is approved. When the entitlement is available, repeat the steps above.
- SelectContinueto launchFactoryTalk® Optix™Studio.TIP:SelectingCancelkeeps theFactoryTalk® Optix™landing page open.To automatically openFactoryTalk® Optix™Studio Pro from your last session, select the avatar with your initials in the upper right corner of the landing page, and then inSettings, selectAuto open last used workspaceand selectSave.NOTE: Once you launchFactoryTalk® Optix™Studio Pro from a browser once, it automatically launches the next time you open theFactoryTalk® Optix™landing page.
Provide Feedback