- FactoryTalk Optix Studio setup
FactoryTalk Optix Studio
Download
FactoryTalk Optix Studio
from the FactoryTalk Optix landing page and install it. Then you can start using it without purchasing an entitlement.- In theReleasessection, selectDownload.NOTE: See FactoryTalk Optix landing page for further details on this subject.
- Select the checkbox next toFactoryTalk Optix Studioand in the upper right corner, select the first instance ofDownload Nowat the top.
- Scroll to read the EULA and selectAccept and Download.The download progress is displayed in theDownload Manager.
- When the download is complete, in the lower left corner, select the up arrow to selectShow in folderand then double-click the.exefile.
- SelectI accept the agreementand complete the setup to installFactoryTalk® Optix™Studio.
FactoryTalk® Optix™
Studio is installed and ready to use.Provide Feedback