Multiple FactoryTalk Optix Studio installations on a single device

Multiple FactoryTalk Optix Studio installations on a single device

Multiple
FactoryTalk® Optix
Studio installations versions can coexist on a single device: newer installations do not automatically replace older ones.
A device can have multiple and simultaneous
FactoryTalk® Optix
Studio instances stored in separate folders named by the version number in the
Program Files
FactoryTalk Optix
repository.
NOTE: More
FactoryTalk® Optix
Studio installations can run at the same time.
Multiple VPN network interfaces install together with their related
FactoryTalk® Optix
Studio installations.
NOTE: If you try to open the same project in another
FactoryTalk® Optix
Studio instance, a warning appears and prevents you from opening it:
The project shares the same name as another project currently open in a different FactoryTalk Optix Studio instance
.
You can log in to GitHub from each
FactoryTalk® Optix
Studio instance by selecting
Settings
Version control
.
When you no longer need a
FactoryTalk® Optix
Studio instance, uninstall it and the related VPN network interfaces.
While installing a newer version of
FactoryTalk® Optix
Studio, a dialog box prompts you to select whether to overwrite older installations.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.