Download Runtime Tools on the Runtime device
Runtime Tools are required on any device running a FactoryTalk Optix application.
They include the
License Manager
and FactoryTalk Optix Application Update Service
.Runtime Tools are embedded in OptixPanel
™
Graphic Terminals by standard, so you do not need to download and install them.If you are using a Runtime device, download Runtime Tools from the FactoryTalk Optix landing page. You can download and install Runtime, including License Manager.
- Access FactorytalkHub.com and select the FactoryTalk Optix tile.
- Authenticate as required. See Authenticate your FactoryTalk Hub account.
- On the FactoryTalk Optix landing page, selectRuntime Tools.
- Scroll down toRuntime Tools Releaseto view the Runtime Tools released versions.
- (optional) To view the FactoryTalk Optix release notes, selectRelease Notes.
- (optional) To view the latest changes in FactoryTalk Optix, selectChangelog.
- (optional) To search for a specific Runtime Tools release, type the release number inSearch.
- To download a specific Runtime Tools release, selectDownloadafter the desired version number, .
- Select the checkbox next to theFactoryTalk Optix Runtime Toolsinstallation package and click on the first instance of the
symbol in the upper right corner. Eventually, click on
Download Now. - Scroll to read the EULA and selectAccept and Download.
- Install theRockwell Automation Download Managerlocated in your Downloads folder. To do so, select
.
Rockwell Automation Download Managerinstalls, runs, and download the Runtime Tools into the specified folder. Download progress is displayed in theRockwell Automation Download Manager. - To determine the Runtime Tools downloading path, after the path, selectChangeto select a different folder.
- Runtime Tools are ready for installation.
Provide Feedback