Install FactoryTalk Optix Runtime Tools on an online device
Once you download the Runtime Tools installation package, install the Runtime Tools.
NOTE:
If the Runtime device is not connected to the Internet, you cannot download the installation package from the FactoryTalk Optix landing page. Download the installation package to an online device and then transfer it to the Runtime device by means of a USB drive.
- When the download is complete, selectOpento open the download folder.
- In the download folder, double-click on FactoryTalk Optix Runtime Tools .exe file and wait for the installation process to complete.The FactoryTalk Optix Application Update Service and FactoryTalk Optix Entitlement Manager are now installed.
NOTE:
If the project includes an ODBC Database linked to a MySQL server, install a
MySQL ODBC connector
additional package that you can download from the Microsoft products page.
NOTE:
If the project includes an ODBC Database linked to an SQL server, install a
ODBC Driver 17 for SQL Server
additional package that you can download from the Microsoft products page.Provide Feedback