System architecture examples

System architecture examples

Runtime entitlements are based on the number of feature tokens that your application requires. The examples given in this section are typical applications; your own architecture may be different than what is shown.
Package sizes:
  • Station Runtime Lite

      XS - extra small; up to 5 tokens

      S - small; up to 8 tokens

  • Station Runtime Standard

      M - medium; up to 11 tokens

      L - large; up to 15 tokens

  • Station Runtime Pro

      XL - extra large; up to 21 tokens

      UNL - unlimited; unlimited tokens

Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal